FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-2
FAQ
FR-A800-2
When the CA output is set as output frequency and the slope is set at 0 to 60 Hz/4 to 20 mA, how does it affect the output when the inverter is reset during 4 mA output?
- Category :
Answer
The output turns OFF (0 mA) during the inverter reset.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800