FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-CRN
FAQ
FR-A800-CRN
It is described that the vibration resistance has been improved. What is the difference with the standard model?
- Category :
Answer
Inverters with the components fixed on the circuit board with an adhesive, an countermeasure against the connector failing, or the cables tied (fixed) together, are available for enhanced vibration resistance.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus