FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-CRN
FAQ
FR-A800-CRN
It is described that the environmental resistance was improved. What does it mean?
- Category :
Answer
The inverter with circuit board coating (conforming to IEC60721-3-3 3C2/3S2) ensures reliability even in poor environments. Furthermore, the inverter with plated conductor is also available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800