FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Life measurement of the main circuit capacitor
FAQ
Life measurement of the main circuit capacitor
Can I turn OFF the power supply only by turning OFF only the main circuit when setting Pr.259 (Main circuit capacitor life measuring) to "1"?
- Category :
Answer
No. Turn OFF and ON both main circuit and control circuit.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800