FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Combination of the FR-A800 and MM-BF
FAQ
Combination of the FR-A800 and MM-BF
When combining the MM-BF and FR-A820, how should I select them?
- Category :
Answer
Select the models so that "MM - BF rated current value × 1.05 < FR-A820 rated output current value".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800