FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Built-in braking resistor
FAQ
Built-in braking resistor
Is the resistance value of the internal resistor of the FR-A800 (7.5K or lower) same as that of the FR-A700?
- Category :
Answer
Yes, the resistance values are the same.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800