FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Vector control
FAQ
Vector control
When the setting of Pr.83 and Pr.84 are enabled? When Pr.71 is set to "30" (Vector control dedicated motor) under Vector control, why is the output voltage not changed by changing Pr.83?
- Category :
Answer
Both settings of Pr.83 and Pr.84 are enabled immediately. However, the output voltage is not changed because the value of Pr.83 has little influence on Vector control. Since the output voltage is calculated from the motor constant, the output voltage is when the motor constant is changed by executing the tuning.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800