FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > JIS standard
FAQ
JIS standard
Is the inverter compliant with the JIS standard?
- Category :
Answer
JIS standard for the inverter is not established. It is required to check whether the whole machine including the inverter is compliant with JIS standard.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, FR-D700, FR-E700, FR-E700EX