FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation panel
FAQ
Operation panel
Can I connect the operation panel to the RS-485 terminal?
- Category :
Answer
No, it cannot be connected to the RS-485 terminal. The 485 terminal supports the Mitsubishi protocol and Modbus-RTU, but it does not support the PU protocol. (The operation panel and parameter unit communicate through PU protocol, which is different from the Mitsubishi protocol.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800