FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > PLC function
FAQ
PLC function
Is the number of timer points 16 for the high speed and low speed in total? Or is it 16 points for each low speed and high speed?
- Category :
Answer
The number of timer points is 16 for the high speed and low speed in total.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800