FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Offline auto tuning
FAQ
Offline auto tuning
What kind of function is the offline auto tuning?
- Category :
Answer
Under Advanced magnetic flux vector control or PM motor control, measuring motor constants automatically enables optimal operation of motors even when motor constants vary, when a motor of another company is used or when the wiring distance is long.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800