FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800
FAQ
FR-A800
The speed response of the vector control (Both with PG/without PG) is improved by more than two times compared to the A700. Is the current response also improved at the same rate?
- Category :
Answer
Yes, the current response is also improved at the same rate.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800