FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Control terminal block
FAQ
Control terminal block
Is the control terminal block of the 500/700 series available for the 800 series?
- Category :
Answer
It is available if the option FR-A8TAT (Control circuit terminal block intercompatibility attachment) is installed. (Some functions have restrictions. For the detail, refer to the Instruction Manual.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800