FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800
FAQ
FR-A800
For the IP55 compatible model, is the operation panel compatible with the IP55?
- Category :
Answer
The operation panel is also compatible with the IP55
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800