FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800
FAQ
FR-A800
Can other manufacturers' magnet motors be used?
- Category :
Answer
By performing offline auto tuning, other manufacturers' IPM, SPM motors can be used under PM sensorless vector control. * When an other manufacturers' magnet motor is used after auto tuning, the starting torque is limited at 50% and zero speed operation or simple positioning control cannot be used. (Tuning may not be available depending on its motor characteristics.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800