FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-BMF
FAQ
FR-BMF
The Instruction Manual instructs includes the following description: "Set Pr.72 "PWM frequency selection" to 2 kHz or less". What happens when 3 kHz or more is set?
- Category :
Answer
The inverter may be broken due to the temperature rise of the internal parts.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option