FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Setting when using the FR-A7AZ and SF-V5RU
FAQ
Setting when using the FR-A7AZ and SF-V5RU
I am planning to use the FR-A7AZ and SF-V5RU with a thermistor. For the model of SF-V5RU ending with A or T, do I have to change any parameters?
- Category :
Answer
Setting of Pr.408 (Thermistor selection) is required. Set as follows. For the model of SF-V5RU ending with "T" (SF-V5RU○○T): Pr.408 = 0 For the model of SF-V5RU ending with "A" (SF-V5RU○○A): Pr.408 = 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Others