FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Wiring length
FAQ
Wiring length
Which capacity, inverter or motor, should be referred for the total wiring length between the inverter and motor?
- Category :
Answer
Refer to the inverter capacity.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700