FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Installation environment
FAQ
Installation environment
It is described that corrosive gas should be avoided for the installation environment. Is there any regulation value (ppm)?
- Category :
Answer
There is no regulation value. Use the inverters in the environment without corrosive gas.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700