FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > EEPROM writing with the communication option
FAQ
EEPROM writing with the communication option
Is the writing on the operation panel written to RAM when Pr.342 (Communication EEPROM write selection) is set to 1 with the communication option?
- Category :
Answer
The writing from the parameter unit or operation panel is always ROM write regardless of the setting value of Pr.342.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700