FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Cumulative power monitoring
FAQ
Cumulative power monitoring
When Pr.170 (Watt-hour meter clear) is set to 0 and cleared, will the data in ROM and RAM be also cleared?
- Category :
Answer
They are cleared as well.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700