FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > LED blinking under encoder feedback control
FAQ
LED blinking under encoder feedback control
When operating the inverter under encoder feedback control, the LED of FWD and REV blinks. What are the possible causes?
- Category :
Answer
The following may be the cause.
- No encoder power supply.
- The setting of Pr.359 (Encoder rotation direction) is reversed.
- The signal from the encoder is not returned normally.
- No encoder power supply.
- The setting of Pr.359 (Encoder rotation direction) is reversed.
- The signal from the encoder is not returned normally.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700