FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Inverter installation when using the FR-A7NCE
FAQ
Inverter installation when using the FR-A7NCE
For the FR-A700 3.7K or lower, the 1 cm or more space is required on its either side. Is it the same when the FR-A7NCE is mounted?
- Category :
Answer
Normally, the required space for A700 3.7K or lower is 1 cm. However, when using CC-Link IE, it needs to be separated for 5 cm or more to pass the cable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P