FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Checking bit state by CC-Link communication
FAQ
Checking bit state by CC-Link communication
Can I check the ON/OFF of the bit from CC-Link communication with monitor code: H0F (input terminal status)?
- Category :
Answer
Because the H0F monitor only observes the ON/OFF of the hardware, it cannot be checked.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700