FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Wiring of CC-Link communication cable
FAQ
Wiring of CC-Link communication cable
This is related to wiring of CC-Link communication cable. In the Instruction Manual of FR-A7NC, the insulator is described that blue is for DA, white is for DB, and yellow is for DG. Can the communication be established even when incorrect color is wired?
- Category :
Answer
The communication is established if DA, DB, and DG are connected each other.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700