FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Parameter copy
FAQ
Parameter copy
How do I copy the parameter to the FR-E500 when replacing the FR-E500 with FR-E700?
- Category :
Answer
The copy function of the parameter unit (FR-PU04) is not available. Setting each parameter again or using the convert function of FR Configurator (FR-SW3-SETUP-WJ) setup software are the only way to copy the parameter.
Please consider to use the setup software.
Please consider to use the setup software.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700