FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Vector control of the inverter
FAQ
Vector control of the inverter
Under Advanced magnetic flux vector control, what happens with the speed fluctuation ratio with/without encoder?
- Category :
Answer
The speed fluctuation ratio under Advanced magnetic flux vector control of the FR-A500 is as follows.
Without encoder: ±1% With encoder (with A5AP): ±0. 02 % (at power driving load)
Without encoder: ±1% With encoder (with A5AP): ±0. 02 % (at power driving load)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500