FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Amount of heat generated
FAQ
Amount of heat generated
Please tell me the amount of heat generated by the E500 series inverter.
- Category :
Answer
The amount of heat generated by the FR-E500 series inverter is registered in the Mitsubishi Electric FA Global Website Member's page.
Refer to the technical news "MF-Z-059" in the technical library.
Refer to the technical news "MF-Z-059" in the technical library.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500