FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Selection method of the reactor
FAQ
Selection method of the reactor
Why and how should I select the reactor between the inverter and motor?
- Category :
Answer
For the use of the 400 V class inverter, the surge voltage suppression filter FR-ASF is provided to suppress the surge voltage occurred at the motor terminal voltage.
Select reactor according to the motor capacity.
Select reactor according to the motor capacity.
- Product Name
- Inverter, magnet motor drive
- Series
- Option