FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Thermal protection
FAQ
Thermal protection
When the optional FR-ABR high-duty brake resistor is installed, is it necessary to provide thermal protection?
I think this is necessary to prevent fire that may occur when the transistor inside the inverter explodes and the resistor temperature goes abnormally high. Am I correct?
I think this is necessary to prevent fire that may occur when the transistor inside the inverter explodes and the resistor temperature goes abnormally high. Am I correct?
- Category :
Answer
Providing thermal protection is better for your safety.
When the brake transistor explodes, the brake transistor alarm (E.BE) is output. Consider a countermeasure using this signal to shut off the inverter power supply.
When the brake transistor explodes, the brake transistor alarm (E.BE) is output. Consider a countermeasure using this signal to shut off the inverter power supply.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024