FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Part selection
FAQ
Part selection
When selecting the inverter FR-A024, the motor capacity and inverter capacity were different.
1. Which capacity (motor or inverter) should be based on when choosing a circuit breaker?
2. Which capacity (motor or inverter) should be based on when choosing a brake resistor?
3. Which capacity (motor or inverter) should be based on when choosing an AC reactor?
1. Which capacity (motor or inverter) should be based on when choosing a circuit breaker?
2. Which capacity (motor or inverter) should be based on when choosing a brake resistor?
3. Which capacity (motor or inverter) should be based on when choosing an AC reactor?
- Category :
Answer
1. Choose the circuit breaker based on the inverter capacity.
2. Also, choose the brake resistor based on the inverter capacity.
3. Choose the AC reactor based on the motor capacity.
2. Also, choose the brake resistor based on the inverter capacity.
3. Choose the AC reactor based on the motor capacity.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024