FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Difference between use with A100 and other types
FAQ
Difference between use with A100 and other types
I use the FR-BLF line noise filter.
The list of options on the catalog explains that two or more filters should be used when the wire is too thick to cover with a single filter for the A100. However, it instructs to use four or more filters for the A200 or A500.
Can I use four filters also for the A100?
Or, is it OK to use fewer filters for the A100 considering the relationship with the inverter?
The list of options on the catalog explains that two or more filters should be used when the wire is too thick to cover with a single filter for the A100. However, it instructs to use four or more filters for the A200 or A500.
Can I use four filters also for the A100?
Or, is it OK to use fewer filters for the A100 considering the relationship with the inverter?
- Category :
Answer
Similarly to the FR-A200 and A500, four or more filters should be used also for the FR-A100.
In short, it is OK if the wire penetrates the filter four times. (For certain wire sizes, two filters will do by winding the wire around the filter two times.)
In short, it is OK if the wire penetrates the filter four times. (For certain wire sizes, two filters will do by winding the wire around the filter two times.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Noise filter
- Series
- Option