FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Heat generation quantity of FR-A500
FAQ
Heat generation quantity of FR-A500
What is the heat generation quantity of the FR-A520-5.5K?
(What is the difference between the A500 and A200E?)
(What is the difference between the A500 and A200E?)
- Category :
Answer
The heat generation quantity of the FR-A520-5.5K is 310 W.
(Reference: The heat generation quantity of the FR-A220E-5.5K is 330 W.)
For other capacities, refer to the FR-A500 technical material.
(Reference: The heat generation quantity of the FR-A220E-5.5K is 330 W.)
For other capacities, refer to the FR-A500 technical material.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500