FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Combination with power factor improving reactor
FAQ
Combination with power factor improving reactor
Can it be combined with the power factor improving reactor?
- Category :
Answer
It cannot be combined with the power factor improving reactor. (Since the power factor is further improved by the high power factor converter, it is not required.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option