FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Can I use the parameter unit FR-PU02?
FAQ
Can I use the parameter unit FR-PU02?
Can I use the parameter unit FR-PU02?
- Category :
Answer
Yes, but functions are partially limited. (The FR-PU02 cannot demonstrate its full ability. The FR-PU01 cannot be used.)
To use the parameter unit FR-PU02, use the connection cable FR-CBL (option).
To use the parameter unit FR-PU02, use the connection cable FR-CBL (option).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024