FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter unit FR-PU03
FAQ
Parameter unit FR-PU03
Can I use the parameter unit FR-PU03 with the FR-A, FR-Z, and FR-U series?
- Category :
Answer
You can use it with the FR-A200 (E) and FR-A100 (E) series.
(Note) Use the connection cable (option).
You cannot use it with the FR-Z and FR-U series (except for the PU operation type).
(Note) Use the connection cable (option).
You cannot use it with the FR-Z and FR-U series (except for the PU operation type).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024