FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Installation of new serial communication unit FR-CU03
FAQ
Installation of new serial communication unit FR-CU03
Where should I install the new serial communication unit FR-CU03?
- Category :
Answer
Remove the parameter unit FR-PU03 and install there. (The installation dimensions of the FR-CU03 are the same as the FR-PU.)
You can read and write parameters as well as start and stop the inverter via the communication cable from a personal computer.
You can read and write parameters as well as start and stop the inverter via the communication cable from a personal computer.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024