FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > How much low-speed torque can be output?
FAQ
How much low-speed torque can be output?
How much low-speed torque can be output?
- Category :
Answer
By choosing the General-purpose magnetic flux vector control and slip compensation function, you can output torque of 150% or more at 1 Hz (200% or more at 3 Hz). (Maximum short-time torque)(For the Mitsubishi standard motor 4P)
For the Mitsubishi standard motor 0.4 to 1.5 kW 4P, continuous 100% torque operation at 6 to 60 Hz is possible in combination with General-purpose magnetic flux vector control.
For the Mitsubishi standard motor 0.4 to 1.5 kW 4P, continuous 100% torque operation at 6 to 60 Hz is possible in combination with General-purpose magnetic flux vector control.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024