FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Comparison of noise with FR-A200
FAQ
Comparison of noise with FR-A200
Does the FR-A200EXCELLENT produce less noise than the FR-A200?
- Category :
Answer
The setting ranges of the carrier frequency are:
- FR-A200: 2 kHz to 14.5 kHz
- FR-A200EXCELLENT: 0.7 kHz to 14.5 kHz
The range of the FR-A200E is extended to the lower side, meaning that you can set the carrier frequency lower than the FR-A200.
This means that noise can be reduced than the FR-A200.
However, for the same carrier frequency, the noise levels are almost same.
- FR-A200: 2 kHz to 14.5 kHz
- FR-A200EXCELLENT: 0.7 kHz to 14.5 kHz
The range of the FR-A200E is extended to the lower side, meaning that you can set the carrier frequency lower than the FR-A200.
This means that noise can be reduced than the FR-A200.
However, for the same carrier frequency, the noise levels are almost same.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200