FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Do you have an explosion-proof type?
FAQ
Do you have an explosion-proof type?
Do you have an explosion-proof type of inverter?
- Category :
Answer
We offer the FR-A200E-based pressure-resistant explosion-proof motor driving inverter FR-B series.
This series have been certified in the explosion-proof test in combination with a specified model of pressure-resistant explosion-proof motor.
As the inverter does not have an explosion proof structure, install it in a non-hazardous place.
This series have been certified in the explosion-proof test in combination with a specified model of pressure-resistant explosion-proof motor.
As the inverter does not have an explosion proof structure, install it in a non-hazardous place.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200