FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Compatibility of the installation between FR-A200EXCELLENT and FR-A200?
FAQ
Compatibility of the installation between FR-A200EXCELLENT and FR-A200?
Are the FR-A200EXCELLENT and FR-A200 compatible in installation?
- Category :
Answer
Yes. (However, since they are aligned with the small size of the FR-A200 (D), you need to use the intercompatibility attachment FR-AAT for a larger size.
Attaching this attachment to the inverter increases the depth of the inverter for 12 to 15 mm.
The following four types require the attachment:
FR-AAT-02 for FR-A220-11K
FR-AAT-10 for FR-A220-45K
FR-AAT-09 for FR-A240-30K
FR-AAT-10 for FR-A240-45K
(The FR-A220D-11K does not require the attachment.)
Attaching this attachment to the inverter increases the depth of the inverter for 12 to 15 mm.
The following four types require the attachment:
FR-AAT-02 for FR-A220-11K
FR-AAT-10 for FR-A220-45K
FR-AAT-09 for FR-A240-30K
FR-AAT-10 for FR-A240-45K
(The FR-A220D-11K does not require the attachment.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200