FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-E740
FAQ
FR-E740
What is the amount of heat generated for each of the capacities from FR-E740-0.4K to 15K?
- Category :
Answer
The following is the amount of heat generated for each capacity:
0.4K: 40W 0.75K: 55W 1.5K: 90W 2.2K: 100W
3.7K: 180W 5.5K: 240W 7.5K: 300W 11K: 400W
15K: 500W
0.4K: 40W 0.75K: 55W 1.5K: 90W 2.2K: 100W
3.7K: 180W 5.5K: 240W 7.5K: 300W 11K: 400W
15K: 500W
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700