FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-E720
FAQ
FR-E720
What is the amount of heat generated for each of the capacities from FR-E720-0.1K to 15K?
- Category :
Answer
The following is the amount of heat generated for each capacity:
0.1K: 14W 0.2K: 20W 0.4K: 32W 0.75K: 50W
1.5K: 80W 2.2K: 100W 3.7K: 160W 5.5K: 290W
7.5K: 380W 11K: 520W 15K: 600W
0.1K: 14W 0.2K: 20W 0.4K: 32W 0.75K: 50W
1.5K: 80W 2.2K: 100W 3.7K: 160W 5.5K: 290W
7.5K: 380W 11K: 520W 15K: 600W
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700