FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Running frequency, output current
FAQ
Running frequency, output current
I want to connect the running frequency and output current to instruments to read them.
- Category :
Answer
Since the FR-E700 has only one terminal FM, you cannot read two signals simultaneously.
Use the optional digital output/additional analog output FR-A7AY.
This option allows for reading two signals simultaneously.
Use the optional digital output/additional analog output FR-A7AY.
This option allows for reading two signals simultaneously.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700