FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link
FAQ
CC-Link
By attaching the CC-Link optional card FR-A7NC E kit, how long does the depth of the inverter increase?
- Category :
Answer
By attaching the optional card and dedicated cover, the depth increases by approximately 15 mm for the FR-E700, and approximately 22 mm for the FR-E700-SC.
Since the terminal block protrudes from the front cover, the depth further increases by approximately 2 mm (2.8 mm at the maximum).
Since the terminal block protrudes from the front cover, the depth further increases by approximately 2 mm (2.8 mm at the maximum).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700