FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Terminal assignment
FAQ
Terminal assignment
I want to assign the AU signal for terminal 4 input selection with the FR-E700.
I do not use the terminal MRS and I want to assign AU to this terminal. How can I do that?
I do not use the terminal MRS and I want to assign AU to this terminal. How can I do that?
- Category :
Answer
The terminal MRS assignment parameter is Pr.183. Set Pr.183 to "4" (AU). (This setting is for the E700.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700