FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-E700
FAQ
FR-E700
I want to attach the CC-Link option FR-A7NC to the FR-E700.
Can I use a DIN rail to install the inverter?
Can I use a DIN rail to install the inverter?
- Category :
Answer
Install the DIN rail attachment to each inverter.
The optional FR-A7NC is built in the inverter and does not influence installation of the inverter.
The optional FR-A7NC is built in the inverter and does not influence installation of the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700