FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link
FAQ
CC-Link
I installed the CC-Link option FR-A7NC on the E700.
Can I change only the acceleration/deceleration time using the optional parameter unit FR-PU07?
Also, how can I use USB connection to allow for operating from the FR-Configurator?
Can I change only the acceleration/deceleration time using the optional parameter unit FR-PU07?
Also, how can I use USB connection to allow for operating from the FR-Configurator?
- Category :
Answer
Set Pr.550 (NET mode operation command source selection) to "2" (PU connector is the command source).
When operating the inverter using the USB connector, set Pr.551 (PU mode operation command source selection) to "3" (USB connector is the command source).
When operating the inverter using the USB connector, set Pr.551 (PU mode operation command source selection) to "3" (USB connector is the command source).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700