FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > 400 Hz output setting
FAQ
400 Hz output setting
Which parameter should I change to change the output to 400 Hz?
- Category :
Answer
Change Pr.18 (High speed maximum frequency) to 400 Hz.
If you are using the analog command to set the frequency, calibrate the 400 Hz frequency with Pr.903.
If you are using the analog command to set the frequency, calibrate the 400 Hz frequency with Pr.903.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500