FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Selection of high-duty brake resistor
FAQ
Selection of high-duty brake resistor
I use a 5.5 kW motor with the FR-E520-7.5K, but the braking efficiency is not sufficient and I want to attach the high-duty brake resistor. Should I select the high-duty brake resistor according to the motor capacity or inverter capacity?
- Category :
Answer
Select the high-duty brake resistor according to the inverter capacity.
- Product Name
- Inverter, magnet motor drive
- Series
- FR-E500, FR-A500